Quick_Stop_deceleration
| Index.Sub | 6085.0H |
| Data Type | Unsigned32 |
| Access | Read/Write |
| PDO Mappable | No |
| Unit | User-defined acceleration unit (1) |
|
Range |
Unsigned32 |
| Default Value | 20000 |
| Store Supported | No |
| Description | This object sets the deceleration ramp used to stop the motor if the 'Quick Stop' command is given and the Quick_stop_option_code is set to 2. |
|
Notes |
(1) See Factor Group. |